This video demonstrates setting up Microsoft Entra ID as an external provider in C•CURE v3.10.
Author: Al Verrier
Installing and Configuring Auth in C•CURE v3.10
This video covers the installation and configuration of Auth in CCURE v3.10.
Incident Management v3.10.1: Configuring a Workflow
This video outlines the steps to create a custom workflow that can be assigned to specific events for effective incident management in C•CURE IQ v3.10.1.
Incident Management v3.10.1
This video demonstrates the new Incident Management feature in C•CURE IQ v3.10.1. An incident is a critical event that poses risk to safety, security, or operations and requires coordinated response, documentation, and accountability. Elevating incidents from events transforms noise into action, ensuring high-impact situations are prioritized, managed through defined procedures, and resolved with clarity and… Continue reading Incident Management v3.10.1
v3.10 C•CURE Converting a Cluster from TLS 1.2 to TLS 1.3 Encryption (one-step conversion)
This video demonstrates how to convert a controller using TLS 1.2 Encryption to TLS 1.3 Encryption in C•CURE 9000 v3.10.
LPR Integration Parking Management Demonstration
This video demonstrates how the LPR integration for CCURE 9000 is used for parking management, including triggering events based on car park activity.
Parking Management LPR Integration Configuration
This video covers the installation of the JCI LPR Integration and the configuration steps in CCURE 9000.
C•CURE Service Account Requirements
Enterprise systems or standalone systems with remote SQL require the use of a Windows service account for Crossfire services. This account has specific requirements. If these requirements are not met, undesired behavior could occur.