Category: C•CURE ID Badging Solutions
C•CURE 800/8000 10.0 C•CURE ID User Guide
C•CureID Image Blending Out with MagiCard Badge Printers
April 16, 2009 PROBLEM With the new version of C•CureID implemented in C•CURE 9000 v1.90, v1.91, and later, the default settings of MagiCard Printers can cause the image on a badge to look washed out, and the image to appear gradient on the edges. SOLUTION: The solution is as follows and only applies to MagiCard… Continue reading C•CureID Image Blending Out with MagiCard Badge Printers