Administration Station Error: Incorrect Syntax near the Keyword ‘Order’

Article ID: SWH-KB-nID-000006848Applies To: C•CURE 9000 (General)Version: 2.90     Symptom(s) Following an upgrade of CCURE from 2.6x to 2.9x, the following error message appears after opening the Administration Station application: Error: Incorrect syntax near the keyword ‘ORDER’. Invalid usage of the option next in the FETCH statement.   The same error will appear in SystemTrace:  <ACVS_M>DataServiceEngine.FindCollection Error:… Continue reading Administration Station Error: Incorrect Syntax near the Keyword ‘Order’

Configuring the iStar Ultra GCM NIC #2 to Connect to IPACMv2

Article ID: SWH-KB-nID-000006821Published: 3-18-2022     Description This document describes how to configure the iStar Ultra to use the second NIC port of the GCM, on a different subnet route than NIC #1, to communicate with an IPACMv2.     Process Confirm that the iStar is running FW 6.8.2.CU02 or newer. The “About” section of the… Continue reading Configuring the iStar Ultra GCM NIC #2 to Connect to IPACMv2