Article ID: 000038187 Date Published: 27/10/2025 Warning – Level 2 Document – Do Not Distribute FAQs 1. What is “CopperApps” in Access-ER?2. Which two mobile apps are required from CopperApps to use GoReader successfully?3. What is the “Barcode Manager” app in Access-ER?4. What is Access ER with MIFARE & MIFARE DESFire Support?5. How to differentiate… Continue reading GoReader FAQ
Category: FAQ’s
C•CURE S300 FAQ and Troubleshooting Supplement
TLS 1.2 to 1.3 Encryption and Default to Host-Based Conversion FAQ
C•CURE 9000 Upgrade Center
IMPORTANT: Read Before Upgrading to C•CURE 9000 Version 3.00 You can upgrade your system directly to C•CURE 9000 v3.00 from the following versions: v2.80 or v2.90. The same HostID value will be used. You can now obtain your licenses online prior to upgrading from the following paths: 2.70 to 2.80 2.70 to 2.90 2.80… Continue reading C•CURE 9000 Upgrade Center