Tag: Integration
3.00 ITv2 Integration for C•CURE 9000 Release Notes
Parking Management LPR Integration Configuration
This video covers the installation of the JCI LPR Integration and the configuration steps in CCURE 9000.
HID 3.0 Integration — Upgrade from C•CURE 9000 2.90 to 3.0 removes UDF’s
Article ID: SWH-KB-000038335 Summary During upgrades from HID Integration 2.9 to 3.0, some sites report issues with previously stored personnel details (custom user-defined fields/UDFs). Engineering has provided an SQL patch to automatically create or update the required UDFs during the upgrade. This patch is validated for both upgrade and fresh install scenarios and performs as expected. Symptoms Custom fields (UDFs) associated with HID data mapping do… Continue reading HID 3.0 Integration — Upgrade from C•CURE 9000 2.90 to 3.0 removes UDF’s
GoReader FAQ
Article ID: 000038187 Date Published: 27/10/2025 Warning – Level 2 Document – Do Not Distribute FAQs 1. What is “CopperApps” in Access-ER?2. Which two mobile apps are required from CopperApps to use GoReader successfully?3. What is the “Barcode Manager” app in Access-ER?4. What is Access ER with MIFARE & MIFARE DESFire Support?5. How to differentiate… Continue reading GoReader FAQ
C•CURE 9000 v3.10 with P2000 Option S321-IP Integration Release Note
RN-CC9K-v3.10-S321-IP-A16383BBPY-A
C•CURE 9000 v3.10 with P2000 Option CK721-A Integration Release Note
RN-CC9K-v3.10-CK721-P2K-A16383BBPU-A