Expiration of C•CURE 9000 Default Certificate for TLS 1.2 Communications to iSTAR Access Controllers

C•CURE 9000 CLOUD RECOMMENDATIONS

Article ID: SWH-TechRef-000024728 Nowadays, more and more businesses intend to host systems in the cloud to reduce large capital expenditure on hardware and upgrades, drive down IT cost, and to increase operational efficiency, agility, and flexibility of their systems. The C•CURE 9000 access control system can be part of the cloud solution. This White Paper… Continue reading C•CURE 9000 CLOUD RECOMMENDATIONS

C•CURE 9000 Virtual Machine Recommendations

Article ID: SWH-TechRef-000024729 This White Paper contains basic recommendations for VM configuration for optimal performance when running the C•CURE 9000 server. It does not contain instructions for the configuration of any particular VM. For information on the configuration of a particular VM, refer to documentation from your VM provider. The focus of this document is… Continue reading C•CURE 9000 Virtual Machine Recommendations

C•CURE 9000 NETWORK BANDWIDTH AND LATENCY RECOMMENDATIONS

Article ID: SWH-TechRef-000024727 This White Paper provides an overview on how network bandwidth and latency affect C•CURE 9000 system. The C•CURE 9000 server sends and receives data to and from its clients and other connected hardware devices, primarily via network. Data is sent and received usually under TCP and UDP messages. Any delay in network… Continue reading C•CURE 9000 NETWORK BANDWIDTH AND LATENCY RECOMMENDATIONS

CCURE9000 CrossFire Framework Simulator – Guideline

Article ID: SWH-TECHREF-nID-000035440     INTERNAL     Not to be shared with or distributed to the public. CCURE9000 CrossFire simulator is one of the internal development tools that primarily helps CCURE9000 developers to test journal messages created by CCURE9000 CrossFire during development cycles.  The simulator does not simulate real object state changes and/or object state change sequence workflows.  It… Continue reading CCURE9000 CrossFire Framework Simulator – Guideline