Article ID: SWH-KB-nID-000006849
Published: Oct-20-2022
- First check to see what the current values of the relevant fields in the table are with a SELECT statement.
SELECT ObjectID, MachineName,uri,IPAddress FROM ACVSCore.dbo.ApplicationServer

- To ensure that the ACVSCore.dbo.ApplicationServer table is updated accurately, use a T-SQL statement such as:
UPDATE ACVSCore.dbo.ApplicationServer
SET
MachineName = ‘NewHostName’,
uri = ‘net.tcp:/NewHostName.domain.tld:8999/CrossFire/IClientSession’
WHERE ObjectID = 5000
- When you execute this T-SQ Statement, you should see (1 row affected) in the Messages pane if it was successful.
- If the system is part of an Enterprise, either a MAS or a SAS, the ObjectID will be different, and you must also update the IP Address column as such:
UPDATE ACVSCore.dbo.ApplicationServer
SET
MachineName = ‘NewHostName’,
uri = ‘net.tcp:/NewHostName.domain.tld:8999/CrossFire/IClientSession’,
IPAddress = ‘10.10.10.10’
WHERE ObjectID = 2097152002
CCURE9000_SWH-KB-nID-000006849_lt_en-1.pdf