Article ID: SWH-KB-nID-000006884Published: Oct-06-2022 Symptoms The CrossFire Framework Service on the MAS is taking an excessive amount of memory, ultimately crashing with an Out of Memory exception. When checking the event logs, they show that CrossFire failed due to System.Outofmemoryexception. Version is 2.60.5011.0453. Cause A large number of scheduled reports are being run daily, but… Continue reading CrossFire Service Memory Leak and Out of Memory Exception