Ultra G2 Not Connecting Due To Wrong TLS Setting

Article ID: SWH-KB-nID-000034934 Published: Jun-07-2022 Symptom When configuring a TLS 1.3 cluster for an iSTAR Ultra G2 GCM, if the GCM is configured incorrectly an error such as: Configuration Error:  ‘Ultra G2 is configured as an iSTAR UltraG2 but actual hardware type detected is iSTAR Ultra Encrypted’ Cause This is caused by the GCM being… Continue reading Ultra G2 Not Connecting Due To Wrong TLS Setting