Update Journal Status for Unified Journals Restored Outside of the Administration Workstation or the Server Configuration Application

Article ID: SWH-KB-nID-000035062

INTERNAL

Problem

When you restore a Unified Journal via SSMS when attempting to manipulate it via Unified Journal Volume Management, it may be stuck in a Running state and not allow you to activate the journal or perform other tasks on it.

Solution

Shut down Crossfire and then run the following SQL script via SSMS:

UPDATE ACVSCore.dbo.ACVSUJournalVolumeManagement
SET DbStatus = 1
WHERE DbExists = ‘Online’
AND DbStatus NOT IN ( 1,2,3)
 

Start Crossfire again. You should be able to perform tasks on the Unified Journal via Unified Journal Volume Management.

INTERNAL_SWH-KB-nID-000035062_lt_en