Article ID: SWH-KB-000038127 Affected Versions Versions prior to C•CURE 3.10 with GO Reader Integration. Summary When using the GO Reader in Roll Call mode, the system does not differentiate between cards with the same card number but different facility codes. This can result in incorrect identification and tracking during roll call operations. Symptoms GO Reader in Roll Call… Continue reading GoReader in Roll Call mode does not recognize Facility Code
Tag: Go
2.90 C•CURE 9000 C•CURE Go Release Note
Article ID: SWH-TECHREF-nID-000006589 Version: 2.90 Published: Jul-1-2021 CC9K-v2-90-CCUREGo-RN-8200-1950-17-A0-en
2.70 C•CURE 9000 C•CURE Go Release Notes
Article ID: SWH-TECHREF-nID-000006639 9000-2-70-ccure-go_rn_lt_en_8200-1525-45a0
.Net Framework 4.5 gives error during C•CURE GO installation
March 12, 2015 BACKGROUND Installing C•CURE GO integration on Windows Server 2012 R2 fails because .Net 4.5 is not detected Please see C•CURE TAB 2015-04 for a variation of this issue. SOLUTION This issue is resolved going forward in C•CURE v2.30R2 ServicePack1. Customers currently experiencing this issue will need to download the updated installer from… Continue reading .Net Framework 4.5 gives error during C•CURE GO installation