Article ID: SWH-KB-nID-000017564 Published: Mar-29-2022 Symptom Following a conversion of a SAS to Standalone, personnel records cannot be deleted. The following error is found in both SystemTrace and the Windows Application Event Log: Cause The stored procedure is missing from the ACVSCORE database Solution Pull a copy of the stored procedure ‘ACVSCore.Access.PersonnelCustomCascadeDelete’ from… Continue reading Unable to Delete Personnel Records
Tag: Personnel Record
Easy Access to Personnel ObjectID and GUID Data
Article ID: SWH-KB-nID-00034529 INTERNAL The ACVSCore.access.personnel database table contains two fields that can uniquely identify a C•CURE 9000 personnel record: – ObjectID– GUID Because both of these two fields can uniquely identify a C•CURE 9000 personnel record, they both have the potential to be very useful in various C•CURE 9000 Data Import scenarios where… Continue reading Easy Access to Personnel ObjectID and GUID Data