Article ID: SWH-KB-nID-000017564
Published: Mar-29-2022
Symptom
Following a conversion of a SAS to Standalone, personnel records cannot be deleted.
The following error is found in both SystemTrace and the Windows Application Event Log:

Cause
The stored procedure is missing from the ACVSCORE database
Solution
Pull a copy of the stored procedure ‘ACVSCore.Access.PersonnelCustomCascadeDelete’ from an existing 2.80SP2 ACVSCORE database, and re-create the stored procedure in the affected ACVSCORE database.
No service restarts are necessary.
CCure9000_SWH-KB-nID-000017564.lt_.en_-1.pdf