Article ID: SWH-KB-nID- 000034643
Published: Jan-25-2023
Problem
After running a repair of Victor Application Server, the services may not start, or the system may behave unexpectedly. This can be caused by the repair process replacing updated files from a Service Pack with the original files.
Solution
If a newer Service Pack is available, you can install that. If not, uninstall any Critical Updates installed and then uninstall the most recent Service Pack installed. Then reinstall the Service Pack and any Critical Updates you removed.