Article ID: SWH-KB-nID-000034479
Published: Mar-29-2022
The Johnson Controls 34-bit Cardkey format, which in P2000 is referred to as Standard Wiegand, uses a reverse bit order compared to most other card formats. Select the Must Always Use Reverse Swipe (iSTAR only) radio button to reverse the bit stream.

On the Format Fields tab, select the values as shown in the screen shot.
The values 1, 468 in the Values column of the Card facility code row are sample entries. Please enter the actual facility code(s) used at the reader.