KB Number: SWH-KB-000037874 Issue Cannot set DNS address on an Edge/Ultra G2. When setting the primary, or secondary, DNS address on an Edge G2 controller with firmware 6.9.6, the DNS address reverts to 0.0.0.0 after changes are saved. This behavior has been observed in firmware versions 6.9.3, 6.9.5 and 6.9.6. If connecting to the controller… Continue reading DNS address on an Edge G2/Ultra G2 cannot be changed without changing other IP Settings like Host IP or Gateway IP