Unable to run Queries if Windows PRINT SPOOLER Service isn’t running

Article ID: SWH-KB-000038555 Overview If the Windows PRINT SPOOLER Service isn’t running on the C•CURE server or remote client PC, you won’t be able to run C•CURE 9000 Queries on that PC.  The problem symptoms are as follows: You’ll initially be able to run a Query once after opening the C•CURE Administration application Afterwards, you won’t be… Continue reading Unable to run Queries if Windows PRINT SPOOLER Service isn’t running